PictureAlias Subroutine

Assigns an alias, or nickname, to the current Picture.

Syntax

PictureAliasPictureAlias, [intErrorMode]

Properties

The PictureAlias subroutine syntax has these parts:

Part

Description

PictureAlias

String. The alias that you want to assign to the current picture.

intErrorMode

Integer. (Optional). The error mode.
0 (default) – Allows the subroutines to provide the error messages. Errors are displayed in the form of a message box. If no entry is made for the intErrorMode parameter, the default is used.

1 – Allows the user to handle the error messages. Errors in the subroutines are passed back to the calling routine for handling.

2 – Writes errors to all destinations. No error messages display. Instead, the errors are written to all iFIX destinations, including the Alarm History window destinations using SendOperatorMessage.

 

Example