Open_TCP_Pic_Ex Method
Opens a Tag Control Panel Picture that displays up to 20 of the valid tags associated with the currently selected object. This method allows you to do the same as the Open_TCP_Pic Method, but allows for multiple instances.
Syntax
object.Open_TCP_Pic_Ex (OpenMultipleInstances)
Properties
The Open_TCP_Pic_Ex method syntax has these parts:
Part |
Description |
object |
An object expression that evaluates to an object in the Applies To list. |
OpenMultipleInstances |
Integer. If set to 1 (true) another instance of the picture is opened. If set to 0 (false), no additional instances of this picture are opened. |