Open_QT_Pic_Ex Method
Opens a Quick Trend Picture for the selected object(s) with a set of pens based on the first eight (8) valid tags. This method allows you to do the same as the Open_QT_Pic Method, but allows for multiple instances.
Syntax
object.Open_QT_Pic_Ex (OpenMultipleInstances)
Properties
The Open_QT_Pic_Ex method syntax has these parts:
Part |
Description |
object |
An object expression that evaluates to an object in the Applies To list. |
OpenMultipleInstances |
Integer. If set to 1 (true) another instance of the picture is opened. If set to 0 (false), no additional instances of this picture are opened. |