Opens, or sends a value of 0, to the specified digital block.
Syntax
OpenDigitalPoint[DigitalPoint], [intErrorMode], [bSendMsg]
Properties
The OpenDigitalPoint subroutine syntax has these parts:
Part |
Description |
DigitalPoint |
String. (Optional). The name of the digital block that you want to open. If no block is specified, it opens the digital point associated with the selected object. |
bstrEventName |
Integer. (Optional). The error mode. 1 – Allows the user to handle the error messages. Errors in the subroutines are passed back to the calling routine for handling. 2 – Writes errors to all destinations. No error messages display. Instead, the errors are written to all iFIX destinations, including the Alarm History window destinations using SendOperatorMessage. |
bSendMsg | Boolean. (Optional). If TRUE, the message "value changed byxxx" will be sent to the alarm destinations. If FALSE, the message will be suppressed. |
Remarks
If no block is specified and the selected object does not have an associated digital point, an error message will occur informing the user that the write was not successful.