Checks to see if the node is enabled for electronic signature by determining if the Electronic Signature option is enabled on the node's hardware key, if iFIX security is enabled on the node, and whether bypass signature is in effect. Bypass signature applies when the currently logged in iFIX user has the Electronic Signature-Bypass application feature assigned.
Syntax
object.IsNodeSignEnabled(pbEnabled)
Properties
The IsNodeSignEnabled method syntax has these parts:
Part |
Description |
object |
An object expression that evaluates to an object in the Applies To list. |
pbEnabled |
Boolean. Returns True if signature is enabled on the local node, False if it is not. |
Return Value
This method returns HRESULT. If the HRESULT is a value other than S_OK, VBA generates an error. You can handle this error using the On Error Statement You can find out more information about the error by using Err Object.