GlobalSlowScrollRate Property
Specifies how slowly historical data can be scrolled in run mode.
NOTE: When using any of the Global Time Control or Playback properties, you need to call the System.GlobalTimerApply method after setting the property.
Syntax
object.GlobalSlowScrollRate [= Double]
Properties
The GlobalSlowScrollRate property syntax has these parts:
Part |
Description |
object |
An object expression that evaluates to an object in the Applies To list. |
Double |
The rate at which the object can be scrolled. The unit of measure depends on if the EnableGlobalScrollPercentage Property is enabled. If it is, then the unit of measure is a percentage. If it is not, then it is the unit of measure specified in the GlobalSlowScrollOption property. |
Remarks
This property cannot be set to a value greater than the GlobalFastScrollRate.