GlobalSlowScrollOption Property

Allows you to specify whether the slow scroll rate for historical data in run mode is in days, hours, minutes, or seconds.

NOTE: When using any of the Global Time Control or Playback properties, you need to call the System.GlobalTimerApply method after setting the property.

Syntax

object.GlobalSlowScrollOption [= enumGlobalSlowScroll]

Properties

The GlobalSlowScrollOption property syntax has these parts:

Part

Description

object

An object expression that evaluates to an object in the Applies To list.

enumGlobalSlowScroll

The units in which the Global Time Control can be scrolled when the System object's EnableGlobalScrollPercentage property is False. The enumeration values are as follows:

0 = Days
1 = Hours
2 = Mins
3 = Secs

Remarks

The EnableGlobalScrollPercentage property must be disabled before you can use this property.

Applies To