GetSelectedAlmExt Method

Returns the alarm extension fields (A_ALMEXT1, A_ALMEXT2) for the tag in the currently selected alarm.

Syntax

object.GetSelectedAlmExt(AlmExt1, AlmExt2)

Properties

The GetSelectedAlmExt method syntax has these parts:

Part

Description

object

An object expression that evaluates to an object in the Applies To list.

AlmExt1

String. Returns the string configured in the alarm's first extension field.

AlmExt2

String. Returns the string configured in the alarm's second extension field.

Return Value

Boolean. True if an alarm is selected, False if no alarm is selected.

Remarks

If no alarm is selected, AlmExt1 and AlmExt2 are set to EMPTY.

 

Example

Applies To