Get_Last_Prompt_Value Method Example
The following code provides an example of the Get_Last_Prompt_Value method that appears in the modDynamoUpdater module of the Project_PlugandSolve VBA project.
Public Function UpdateADynamo(objDynamoInstance As Fix2DDynamo.Fix2DDynamo, objMasterDynamo As Fix2DDynamo.Fix2DDynamo, ByRef strReturnMsg) As UpdateDynamoResult
Dim strDIName As String
Dim strDMName As String
Dim iDataSourceOption As DynamoDataSourceOption
Dim iResult As Long 'UpdateDynamoResult
Dim iPrompt As Long
iDataSourceOption = g_WizardConfig.iDataSourceOption
If g_WizardConfig.iDataSourceOption = DYNAMO_PROMPT_FOR_CHOICE Then
If g_ReturnFromPromptForChoice = PROMPT_DLG_SEL_UPDATE_NO_DS_APPLY_TO_ALL Then
iDataSourceOption = DYNAMO_UPDATE_BUT_NOT_APPLY
ElseIf g_ReturnFromPromptForChoice = PROMPT_DLG_SEL_UPDATE_ATTEMPT_MATCH_APPLY_TO_ALL Then
iDataSourceOption = DYNAMO_UPDATE_AND_APPLY
ElseIf g_ReturnFromPromptForChoice = PROMPT_DLG_SEL_DO_NOT_UPDATE_APPLY_TO_ALL Then
iDataSourceOption = DYNAMO_NOT_UPDATE
End If
End If
'////// actual update call
' call Update A Dynamo
PlugandSolve.GeometryHelperObj.Update_A_Dynamo_By_Ref objMasterDynamo, objDynamoInstance, iDataSourceOption, mobjStrMgr.GetNLSStr(4069), iResult
' get a result string
strReturnMsg = PlugandSolve.GeometryHelperObj.Get_Last_Result_String
' get the last user choice from the prompt
If (g_WizardConfig.iDataSourceOption = DYNAMO_PROMPT_FOR_CHOICE) And _
(g_ReturnFromPromptForChoice = PROMPT_DLG_SEL_NONE) Then
iPrompt = PlugandSolve.GeometryHelperObj.Get_Last_Prompt_Value
If (iPrompt = PROMPT_DLG_SEL_UPDATE_NO_DS_APPLY_TO_ALL) Or _
(iPrompt = PROMPT_DLG_SEL_UPDATE_ATTEMPT_MATCH_APPLY_TO_ALL) Or _
(iPrompt = PROMPT_DLG_SEL_DO_NOT_UPDATE_APPLY_TO_ALL) Then
g_ReturnFromPromptForChoice = iPrompt
End If
End If
'////// end of actual update call
'////// dummy for test
' g_testcount = g_testcount + 1
' strDIName = objDynamoInstance.Name
' strDMName = objMasterDynamo.Name
' If g_testcount = 3 Then
' strReturnMsg = ">>>" & strDIName & " was not updated with " & strDMName
' iResult = DYNAMO_NOTUPDATED
' ElseIf g_testcount = 150 Then
' strReturnMsg = ">>> User canceled"
' iResult = DYNAMO_UPDATE_ABORTED
' Else
' strReturnMsg = strDIName & " was updated successfully with " & strDMName
' iResult = DYNAMO_UPDATED
' End If
'////// end of dummy for test
If iResult <= DYNAMO_UPDATED Then
UpdateADynamo = DYNAMO_UPDATED
ElseIf iResult <= DYNAMO_NOTUPDATED Then
UpdateADynamo = DYNAMO_NOTUPDATED
Else
UpdateADynamo = DYNAMO_UPDATE_ABORTED
End If
End Function
To view this
code in context:
- In Classic view, from the WorkSpace menu, select Visual Basic Editor.
-Or-
In Ribbon view, on the Home tab, in the WorkSpace group, click Visual Basic Editor.
- In the tree view, double-click the Project_PlugandSolve folder, and then the Modules folder, and finally the modDynamoUpdater.
- Search for UpdateADynamo to locate this code.