Creates a new Picture.
Syntax
GeneratePicture (aPicInfo)
Properties
The GeneratePicture subroutine syntax has this part:
Part |
Description |
aPicInfo |
The PictureInfo structure specifies the properties of the picture to be generated. |
The members of the PictureInfo structure are as follows:
Member |
Description |
lfTopPct |
The preferred top window edge location of the picture being generated. The location Unit, pixel or percent, is determined by bPixels. Type is Double. |
lfLeftPct |
The preferred left window edge location of the picture being generated. The location Unit, pixel or percent, is determined by bPixels. Type is Double. |
lfHeightPct |
The preferred window height of the picture being generated. The dimension Unit, pixel or percent, is determined by bPixels. Type is Double. |
lfWidthPct |
The preferred window width of the picture being generated. The dimension Unit, pixel or percent, is determined by bPixels. Type is Double. |
lBkColor |
Color for background color of the picture. Type is Long. |
szName |
The name of the picture. Type is String. |
bPixels |
Determines whether the window location units are pixel or percent. Type is Boolean. |
bTitlebar |
Defines whether or not the picture window has a title bar. Type is Boolean. |
bSystemMenu |
Defines whether or not the picture window has a system menu. Type is Boolean. |
bResizable |
Defines whether or not the picture window is resizable. Type is Boolean. |
bAlwaysOnTop |
Defines whether or not the picture window is always on top of other picture windows. Type is Boolean. |
bRuntimeVisible |
Defines whether or not the picture is visible at run time. Type is Boolean. |