Returns the requested iFIX system path for the specified path index.
Syntax
object.FixPath(ePathID as PathID)
Properties
The FixPath property syntax has these parts:
Part |
Description |
object |
An object expression that evaluates to an object in the Applies To list. |
index |
The path index. |
Settings
The settings for PathID are:
Constant |
Value |
Description |
Base_Path |
0 |
Base path. |
Pic_Path |
1 |
Picture path. |
ToolBar_Path |
2 |
Toolbar path. |
Documents_Path |
3 |
Documents path. |
Schedule_Path |
4 |
Schedule path. |
Local_Path |
5 |
Local path. |
Pdb_Path |
6 |
PDB path. |
Nls_Path |
7 |
NLS path. |
App_Path |
9 |
Application path. |
Htc_Path |
10 |
HTC path. |
Htd_Path |
11 |
HTD path. |
Alm_Path |
12 |
Alarm path. |
Rcm_Path |
13 |
RCM path. |
Rcc_Path |
14 |
RCC path. |
Project_Path |
15 |
iFIX project path. |
NOTE: To access these constants, add a reference to the iFIX Global System Information Type Library in the Visual Basic Editor.
Remarks
FixPath is a read-only property of type String.