FixCheckAreaAccessQuiet Method

Checks to see if the user has access to the specified area. The FixCheckAreaAccessQuiet method refrains from sending a security violation message if the user does not have access.

Syntax

object.FixCheckAreaAccessQuiet(Area)

Properties

The FixCheckAreaAccessQuiet method syntax has these parts:

Part

Description

object

An object expression that evaluates to an object in the Applies To list.

Area

Integer. The area that the user is trying to access.

Return Value

Long. Returns 1 if the user has access to the specified area, 0 otherwise.

Remarks

The mapping of area number to area name can be seen in the Security Configurator under area configuration.

 

Example

Applies To