Specifies the maximum pixel length of the space between the line to be extended and the intersection point. If the space is greater than this number, the line will not be extended to the intersection point.
Syntax
object.ExtendMaxSpace [=Integer]
Properties
The ExtendMaxSpace property syntax has these parts:
Part |
Description |
object |
An object expression that evaluates to an object in the Applies To list. |
Integer |
The maximum number of pixels allowed between the line to be extended and the intersection point. |