Enumerate_Top_Level_Groups Method Example
The following code provides an example of the Enumerate_Top_Level_Groups method:
Public Function GetOldDynamoList(objFDS As CFixDynamoSet, ByRef colDMList As Collection) As Boolean
Dim colFDS As CFixObjectCollection
Dim colList As CFixObjectCollection
Dim objDM As Object
If TypeName(objFDS) = "Nothing" Or objFDS.Category <> "Dynamo Sets" Then
GetOldDynamoList = False
GoTo CLEAN_UP
End If
'If objHelper.ClassName <> "GeometryHelper" Then
' GetMasterDynamoList = False
' GoTo CLEAN_UP
'End If
' clear dynamo instance list
Do While colDMList.Count > 0
colDMList.Remove (1)
Loop
' get all Master Dynamos on a specified DynamoSets
Set colFDS = objFDS.ContainedObjects
Call PlugandSolve.GeometryHelperObj.Enumerate_Top_Level_Groups(colFDS, colList)
If colList.Count <= 0 Then
GetOldDynamoList = True
GoTo CLEAN_UP
End If
For Each objDM In colList
colDMList.Add objDM
Next objDM
GetOldDynamoList = True
CLEAN_UP:
On Error Resume Next
Set colList = Nothing
Set colFDS = Nothing
Set objDM = Nothing
End Function