EnhancedCoordinates Property

Read-only. Specifies whether the current picture uses screen independent coordinates (Enhanced Coordinates) or the legacy logical coordinates.  For more information on Enhanced Coordinates, refer the Picture Coordinate Systems topic in the Creating Pictures e-book.

Syntax

object.EnhancedCoordinates [= Boolean]

Properties

The EnhancedCoordinates property syntax has these parts:

Part

Description

object

An object expression that evaluates to an object in the Applies To list.

Boolean

Whether or not Enhanced Coordinates are used.

Settings

The settings for Boolean are:

Value

Description

True

Enhanced Coordinates are used.

False

Enhanced Coordinates are not used.

Remarks

The default for EnhancedCoordinates is True on all new pictures created in iFIX 5.8 and greater. On pictures created in previous versions of iFIX, the default for EnhancedCoordinates is False, unless you choose to upgrade to the Enhanced Coordinate system by running the Picture Upgrade expert and then the property gets set to True.

Applies To