EnableAlarmDeletion Property
Specifies whether alarms can be deleted from the Alarm Summary object.
Syntax
object.EnableAlarmDeletion [= Boolean]
Properties
The EnableAlarmDeletion property syntax has these parts:
Part |
Description |
object |
An object expression that evaluates to an object in the Applies To list. |
Boolean |
Whether alarms can be deleted. |
Settings
The settings for Boolean are:
Value |
Description |
True |
Alarms can be deleted from the Alarm Summary object. (Default) |
False |
Alarms cannot be deleted from the Alarm Summary object. |
Remarks
Setting EnableAlarmDeletion to True allows the user to delete alarms whether they have been acknowledged or not.