Specifies the value representing a shape's edge style.
Syntax
object.EdgeStyle [= enumEdgeStyle]
Properties
The EdgeStyle property syntax has these parts:
Part |
Description |
object |
An object expression that evaluates to an object in the Applies To list. |
EnumEdgeStyle |
The edge style to be displayed for the specified shape. |
Settings
The settings for enumEdgeStyle are:
Constant |
Value |
Description |
EdgeStyleSolid |
0 |
Solid |
EdgeStyleDash |
1 |
Dash |
EdgeStyleDot |
2 |
Dot |
EdgeStyleDashDot |
3 |
Dash-Dot |
EdgeStyleDashDotDot |
4 |
Dash-Dot-Dot |
EdgeStyleNone |
5 |
No border. |
EdgeStyleInsideFrame |
6 |
Inside Frame. |
Bitmap Object Syntax
object.EdgeStyle [= enumBitmapEdgeStyle]
Properties
The EdgeStyle property syntax has these parts:
Part |
Description |
object |
An object expression that evaluates to an object in the Applies To list. |
EnumBitmapEdgeStyle |
The edge style to be displayed for the specified bitmap. |
Object Settings
The settings for enumBitmapEdgeStyle are:
Constant |
Value |
Description |
BitmapEdgeNone |
0 |
No edge. |
BitmapEdgeSunken |
1 |
Sunken edge. |
BitmapEdgeRaised |
2 |
Raised edge. |
BitmapEdgeEtched |
3 |
Etched edge. |
BitmapEdgeBump |
4 |
Bump edge. |
Remarks
Changes to the EdgeStyle property are only visible when the EdgeWidth property of the object is set to 1.