eda_type_to_index Function
Retrieves the type index for the specified string containing a block type.
Syntax
Function eda_type_to_index (NodeName, BlockType)
Properties
The eda_type_to_index function syntax has these parts:
Part |
Description |
object |
An object expression that evaluates to an object in the Applies To list. |
NodeName |
String. Name of node on which the block is located. |
BlockType |
String. The block type whose block index is required. |
Return Value
Integer. The database block type (a value between 1 and 150). Returns 0 if the type name is not recognized.
Remarks
The block index returned by this function should be used when adding blocks to the database via the eda_add_block function.