Deletes the specified database block from the database.
Syntax
Function eda_delete_block (NodeName, TagName)
Properties
The eda_delete_block function syntax has these parts:
Part |
Description |
object |
An object expression that evaluates to an object in the Applies To list. |
NodeName |
String. The node name on which to delete the block. |
TagName |
String. The name of the block to be deleted. |
Return Value
FE_OK if successful; FE_XXX if error.
Remarks
Deletes the specified block from the database. If this block is part of a chain, then the previous and next blocks of the chain will be reconnected. It is good practice to place the block OFFSCAN before deleting it.