Returns a flag signifying whether this OPC DataServer was installed as the default.
Syntax
object.DefaultServer
Properties
The DefaultServer property syntax has this part:
Part |
Description |
object |
An object expression that evaluates to an object in the Applies To list. |
Return Values
The DefaultServer property return values are:
Value |
Description |
0 |
The specified data server is not the default server. |
1 |
The specified data server is the default server. |
Remarks
DefaultServer is a read-only property of type String.
The DefaultServer information is registered during installation of the OPC server using the DataServerInstaller program.