DataRefreshInterval Property

Specifies the rate at which real-time values are retrieved for tags in the current alarm list in the Alarm Summary object.

Syntax

object.DataRefreshInterval [= Single]

Properties

The DataRefreshInterval property syntax has these parts:

Part

Description

object

An object expression that evaluates to an object in the Applies To list.

Single

The rate, in seconds, at which real time values are retrieved for tags in the current alarm list. The valid values are 0.1 - 300.0 The default is 0.5 seconds.

 

Applies To