Coupled_DeActivate_Workspace_UI Method

Determines whether or not a form is modeless in the Configuration environment.

Syntax

object.Coupled_DeActivate_Workspace_UI bLeaveActiveDocActive

Properties

The Coupled_DeActivate_Workspace_UI method syntax has these parts:

Part

Description

object

An object expression that evaluates to an object in the Applies To list.

bLeaveActiveDocActive

Boolean. If True, objects can be selected and moved in the currently active document. The right mouse menu and double click events are disabled. In addition, the active document cannot be moved, closed, maximized, or minimized. If False, objects cannot be selected or moved in the currently active document.

Remarks

User forms are modal by default. To make a form modeless, make the following call on form initialization (in the form's Activate event):

Application.Coupled_Activate_Workspace_UI True

 

This call must be made from a form that is activated by a toolbar script.

 

Example

Applies To