Activates the WorkSpace UI after a Coupled_DeActivate_Workspace_UI method call in the Configuration environment.
Syntax
object.Coupled_Activate_Workspace_UI(bForce)
Properties
The Coupled_Activate_Workspace_UI method syntax has these parts:
Part |
Description |
object |
An object expression that evaluates to an object in the Applies To list. |
bForce |
Boolean. If True, objects can be selected and moved in the currently active document. The right mouse menu and double click events are disabled. In addition, the active document cannot be moved, closed, maximized, or minimized. If False, objects cannot be selected or moved in the currently active document. |
Remarks
This method must be called when the Coupled_DeActivate_Workspace_UI method has been called in VBA scripts that do not involve user forms.