Closes the specified Picture. If there are multiple instances of a picture open, all instances of that picture are closed. If a different alias is assigned to each instance, you can close one instance using an alias.
Syntax
ClosePicture[Picture], [intErrorMode]
Properties
The ClosePicture subroutine syntax has these parts:
Part |
Description |
Picture |
String. (Optional). The file name or alias of the picture you want to close. If no file name is specified, the currently active picture is closed. |
intErrorMode |
Integer. (Optional). The error mode. |