CheckSecurityEnabled Method

Checks if iFIX security is enabled on the local node.

Syntax

object.CheckSecurityEnabled(pbSecurityEnabled)

Properties

The CheckSecurityEnabled method syntax has these parts:

Part

Description

object

An object expression that evaluates to an object in the Applies To list.

pbEnabled

Boolean. Returns True if security is enabled, False if it is not.

Return Value

This method returns HRESULT. If the HRESULT is a value other than S_OK, VBA generates an error. You can handle this error using the On Error Statement You can find out more information about the error by using Err Object.

 

Example

Applies To