CheckAccountExpiration Method
Checks a Windows user account and returns account password expiration information.
Syntax
object.CheckAccountExpiration(bstrUsername, pbExpired, pbCanChangePassword, pnDaysLeft)
Properties
The CheckAccountExpiration method syntax has these parts:
Part |
Description |
object |
An object expression that evaluates to an object in the Applies To list. |
bstrUserName |
String. Specifies the Windows user name. |
pbExpired |
Boolean. Returns True if the Windows user account password is expired, and False if it is not. |
pbCanChangePassword |
Boolean. Returns True if the user is allowed to change their password, and False if he is not. |
pnDaysLeft |
Long. Returns the number of days left until the account password expires. |
Return Value
This method returns HRESULT. If the HRESULT is a value other than S_OK, VBA generates an error. You can handle this error using the On Error Statement You can find out more information about the error by using Err Object.