AlarmRefreshInterval Property

Specifies the rate at which the Alarm Summary object checks for a change in the list of alarms.

Syntax

object.AlarmRefreshInterval [= Single]

Properties

The AlarmRefreshInterval property syntax has these parts:

Part

Description

object

An object expression that evaluates to an object in the Applies To list.

Single

The rate, in seconds, that the Alarm Summary will update the list of alarms. The valid values are 0.1 to 300. The default is 0.5 seconds.

 

Applies To