Toggles the system's AlarmHornEnabled status.
Syntax
AlarmHornEnabledToggle ([intErrorMode])
Properties
The AlarmHornEnabledToggle subroutine syntax has this part:
Part |
Description |
intErrorMode |
Integer. (Optional). The error mode. 1 – Errors are not handled so that they can be handled in the calling routine. 2 – Errors are dispatched to the alarm destinations using SendOperatorMessage. |
Return Value
Boolean. The status of the AlarmHornEnable after the call is completed.
True = The status was toggled to True. The horn will sound on any new alarm.
False = The status was toggled to False. The horn will not sound for any new alarms.