Gets or sets the alarm horn enabled status.
Syntax
AlarmHornEnabled ([blnNewValue], [intErrorMode])
Properties
The AlarmHornEnabled subroutine syntax has these parts:
Part |
Description |
blnNewValue |
Boolean. (Optional). The value to which you want to set the alarm horn enable property. |
intErrorMode |
Integer. (Optional). The error mode. 1 – Errors are not handled so that they can be handled in the calling routine. 2 – Errors are dispatched to the alarm destinations using SendOperatorMessage. |
Return Value
Boolean. The status of the AlarmHornEnable after the call is completed.
True = The horn will sound on any new alarm.
False = The horn will not sound for any new alarms.