Selecting Common Alarm Areas Not Listed in the Database
To select a common
alarm area that is not listed in the alarm area database:
- In Classic view, from the iFIX WorkSpace, click the System Configuration Utility button on the toolbar.
-Or-
In Ribbon view, on the Applications tab, in the System & Security group, click SCU.
- On the SCU toolbox, click the Alarms button.
- Double-click the alarm service you want to set up.
- Click the Areas button.
- Select the Select from Alarm Area Database option.
- In the Add field, enter the area's name and click the Add button.
- Click Yes when prompted to use the undefined name.
See Also
Alarm Configuration Dialog Box
Configure Alarm Areas Dialog Box
Assigning Common Alarm Areas to an Alarm Service
Assigning Every Alarm Area to an Alarm Service
Assigning Every Alarm Area to Application Messages
Assigning Specific Alarm Areas to an Alarm Service