Configuring the SQL Task
To configure
the SQL task:
- In Classic view, from the iFIX WorkSpace, click the System Configuration Utility button on the toolbar.
-Or-
In Ribbon view, on the Applications tab, in the System & Security group, click SCU.
- On the SCU toolbox, click the SQL button.
- Click the Configure SQL Task button.
- Complete the SQL Task Configuration dialog box, as desired.
NOTE: When using the confirm tag for an SQT block that is triggered by an event, make sure that you define the security so that users do not have access to Mission Control to shut down the SQL task.
- Click OK.