Advanced Network Configuration Dialog Box

This dialog box allows you to change the values of the network timers and control LAN redundancy on your node. iFIX uses your entries in this dialog box to tailor resources precisely for your configuration.

CAUTION: Modifying network resources can seriously affect the performance of a node. You should not use this dialog box unless you have a thorough understanding of iFIX networking concepts.

The Advanced Network Configuration dialog box displays the following items:

Network Timers

Field

Description

Keep Alive Field and Check Box

Allows you to specify the amount of time that, if no activity has occurred over an established connection, a View client waits before sending a heartbeat message. The default value for this field is 20 seconds.

Send Field and Check Box

Allows you to specify the amount of time that a View client waits for a request to the SCADA server to be acknowledged. If this timer expires, the session ends. The default value for this field is 30 seconds.

Receive Field and Check Box

Allows you to specify the amount of time that a View client waits for a reply from the SCADA server. When running iFIX over TCP/IP, the effective session timeout values is either the Send timer or the Receive timer, whichever is greater. If this timer expires, the session ends. The default value for this field is 60 seconds.

Inactivity Field and Check Box

Allows you to specify the amount of time that, if no data activity has occurred over an established connection, a View client waits before removing the dynamic connection from the list of outgoing connections. If this timer expires, the session ends. The default value for this field is 300 seconds.

Reset to Defaults Button

Allows you to reset the network timers to their default values.

NOTE: See the Determining Session Timer Values section in the Setting up the Environment electronic book for more information on network timers.

LAN Redundancy

Field

Description

Available Paths List

Displays a list of available network paths.

Enable Status Option Button

Allows you to enable the network path selected in the Available Paths list box for LAN redundancy.

Disable Status Option Button

Allows you to disable the network path selected in the Available Paths list box for LAN redundancy.

Enable LAN Redundancy Check Box

Allows you to enable the LAN redundancy feature on the node.

Reset to Defaults Button

Allows you to reset LAN redundancy to its default values.

More Network Options

Field

Description

Accept Unknown Host

Select this option to allow the SCADA node to accept connections from any computer. When the parameter is disabled, access is restricted to the iClients (View) you specify.

Accept Unauthorized Writes

Select this option to allow the SCADA node to log all unauthorized write attempts from the iClients.

Log Unauthorized Writes

Select this option to enable the logging of failed writes.

Edit Box

Allows you enter a node name to add to the Hosts or Write Nodes list.

Add Hosts Button

Click the button to add a node from the above edit box to the Hosts list.

Remove Host

Select a host in the list and then click this button to remove it from the list.

Add Write Node Button

Click the button to add a node from the above edit box to the Write Nodes list.

Remove Node

Select node that allows writes in the list and then click this button to remove it from the list.

Hosts List

Displays a list of hosts.

Write Nodes List

Displays a list of writable nodes.

 

How Do I...