To run iFIX as
a service under Microsoft Windows:
- Shut down iFIX.
- Make sure that you are logged in as a user in the Administrators group. If not, log in as an Administrator now.
- On the Start menu, point to Programs, iFIX, and then System Configuration. The System Configuration Utility (SCU) window appears.
- In the SCU, on the Configure menu, click Local Startup. The Local Startup Definition dialog box appears.
- In the Service area, select the Run iFIX as a Service check box.
NOTE: The check boxes in the Service area of this dialog box are unavailable while iFIX is running. You need to shut down iFIX, as you did in step 1, to update them. For more information on running iFIX as a service, see Running iFIX as a Service in the Getting Started guide.
- If you want iFIX to start automatically whenever the Windows starts, select the Set Service Startup Type to Automatic check box.
- Click OK.
- On the File menu, click Save.
- Close the SCU.
- Restart iFIX.