Configuring Network Protocols
To configure
the network protocol:
- In Classic view, from the iFIX WorkSpace, click the System Configuration Utility button on the toolbar.
-Or-
In Ribbon view, on the Applications tab, in the System & Security group, click SCU.
- On the SCU toolbox, click the Network button.
- In the Network area, click TCP/IP to configure the network protocol. If you do not want to be connected to a network, click No Network Support. This option configures iFIX to operate as a stand-alone server.
- Click OK.