To configure
a task to start automatically:
- In Classic view, from the iFIX WorkSpace, click the System Configuration Utility button on the toolbar.
-Or-
In Ribbon view, on the Applications tab, in the System & Security group, click SCU.
- On the SCU toolbox, click the Tasks button.
- Click the browse (...) button next to the Filename field.
- Select the desired file and click the Open button. The selected file appears in the Filename field.
- In the Startup Mode area, click the Normal option button to start the task as an open window, the Minimized option button to start the task as a minimized window, or the Background option button to start the task in the background.
- In the Command Line field, enter any command line parameters you may need.
- Click the Add button to add the task to the Configured Tasks list box.
- Click the up or down arrow buttons to move the task in the list.
- Click OK.