To remove all
startup profiles:
- In Classic view, in the iFIX WorkSpace, on the toolbar, click the Startup Profile Manager button.
-Or-
In Ribbon view, on the Applications tab, in the Utilities group, click Utilities, and then click Startup Profile Manager.
NOTE: The Startup Profile Manager can also be accessed from the Start menu by pointing to Programs, iFIX, Tools, and then Startup Profile Manager.
- On the File menu, click Remove All Profiles.
- Click Yes to continue. The startup profile list in the main screen appears empty after the profiles are removed.
NOTE: The settings defined in the Default Startup Profile dialog box are not removed. Only startup profiles in the list that appears in the main window are removed.
- On the File menu, click Save.
See Also