Starting and Exiting the SCU

To properly start and configure the SCU, you should do so before you open the iFIX WorkSpace. You can start the SCU by clicking Start and pointing to Programs, iFIX, and then System Configuration. However, if you are in the iFIX WorkSpace and you need to make changes, you can start the SCU by clicking the SCU button on the Application toolbar (Classic view), or on the Applications tab, in the System & Security group, click SCU (Ribbon view), or by double-clicking System Configuration in the system tree. Note that, for its first startup, the SCU uses the node name you specified during installation.

The main SCU window displays graphics and icons that represent enabled options and tools. You can click many parts of the window to bring up the related dialog box. This graphical interface lets you determine at a glance what kind of node and options the open SCU file enables. You can also disable an option by selecting the graphic or icon in the main SCU window and pressing Delete.

NOTE: Deleting an icon from the main SCU window removes that service from your server's configuration. A dialog box appears warning you of this.

 

See Also