Increasing the Refresh Rate

The steps that follow explain how to increate the refresh rate of an object.

To increase the refresh rate of an object:

  1. Double-click the object you want to modify.
  2. Click the Browse button to the right of the Data Source field.
  3. In the Refresh Rate field, click the drop down menu and choose a rate number that is smaller than your current refresh rate.
  4. Switch to the run-time environment, to make sure sessions are not lost and that alarms are received in a timely manner.

    If sessions are being lost or alarms are not received in a reasonable amount of time, increase the refresh rate in 1 second increments until sessions are not lost and alarms are received without delay.

 

See Also

How Do I...