At the top of the SCU window, a short title appears under the menu bar. This is the name of your SCU file, also known as a file description. You can change the name so that each SCU file has a unique identifier. The file description is only there to help you distinguish between SCU files; the system does not use the description in any way.
To name your SCU file, select Description from the File menu, or double-click the title area. Enter a description of up to 40 characters in the Enter Configuration File Description field.