Edit Startup Profile Dialog Box

The Edit Startup Profile dialog box displays the following items:

iFIX Nodename

Enter the iFIX node name that you want to associate with this user.  This name can up to eight characters long.  

SCU File

Enter the location and name of the SCU file that you want the specified Windows user to use when starting iFIX.  Optionally, click the Browse (…) button to search for a file.   

iFIX Startup Options

Item

Description

Allow User to Run Sample System

Select this check box if you want to allow the specified Windows user to run the iFIX Sample System.  Uncheck this option if you want to deny the use of the sample system to the specified user.

By default, this check box is selected.   

NOTE: As of iFIX 5.8, the Sample System is no longer shipped with iFIX. Be aware that the Sample System is not supported in iFIX 5.8 and greater.

Allow User to Modify Nodename and SCU

Select this check box to allow the specified Windows user to edit the SCU or node name from the iFIX Startup dialog box.  Uncheck this option if you want to make these fields unavailable when the user starts iFIX.

By default, this check box is selected.   

How Do I...