Enabling TCP/IP Networking for the Auto Alarm Manager
To enable TCP/IP
networking on the Sender and Receiver nodes:
- Shut down iFIX if it is running.
- On the Start menu, point to Programs, iFIX, and then System Configuration. The SCU application appears.
- On the Configure menu, click Network. The Network Configuration dialog box appears.
- In the Network group box, select the TCP/IP option.
- Click OK.
- On the File menu, click Save.
- Exit the SCU.
NOTE: It does not matter whether you have the Dynamic Connections check box selected or Remote Nodes added to the list box. The Auto Alarm Manager will work with any settings here.
NOTE: Be sure to repeat steps 1-7 on both the Sender and Receiver nodes.