Network
Status Display (NSD) Fields
Field Name
|
Description
|
A_ACONNREASON_0 through A_ACONNREASON_200
|
The current state of the connection to the active
node. This is either "Established" or text describing the current
state.
|
F_ACTIVECLIENTS |
The total number of connected view nodes. |
A_ACTIVEPATH_0 through A_ACTIVEPATH_200
F_ACTIVEPATH_0 through F_ACTIVEPATH_200
|
Indicates if the active path is the primary or secondary
path.
A 0 in this field indicates that the primary path
is the active path; a 1 indicates that the backup path is the active path.
|
A_ACTIVESCADA_0 through A_ACTIVESCADA_200
|
Active SCADA Server name, which can be either the
primary or secondary node name.
|
A_ACTIVESTATUS_0 through A_ACTIVESTATUS_200
F_ACTIVESTATUS_0 through F_ACTIVESTATUS_200
|
Status of the connection to the active SCADA (OK or
an error code). It will be one of the primary, logical, or secondary statuses.
|
A_ALOCALADDR_0 through A_ALOCALADDR_200
|
This is for the active network connection. For TCP/IP,
displays the local IP address used to reach the remote node.
|
F_ALLOWREMOTEWRITES_0 through F_ALLOWREMOTEWRITES_200
|
This field is 1 if remote nodes are allowed to write to the NSD
fields on the active node, or 0 if writes are not allowed.
|
A_APATHSTATUS_0 through A_APARTHSTATUS_200
F_APATHSTATUS_0 through F_APATHSTATUS_200
|
Status of the connection over the active path. This
is either the primary or secondary status.
|
A_AREMOTEADDR_0 through A_AREMOTEADDR_200
|
This is for the active network connection. For TCP/IP,
displays the IP address of the remote node.
|
A_BACKUPPATH_0 through A_BACKUPPATH_200
|
Backup network path. When using LAN Redundancy, it
shows the paths per connection. For TCP/IP,
it is the IP address.
|
A_BACKUPSCADA_0 through A_BACKUPSCADA_200
|
Standby SCADA Server name for this connection.
|
A_BACKUPSTATUS_0 through A_BACKUPSTATUS_200
F_BACKUPSTATUS_0 through F_BACKUPSTATUS_200
|
Status of the connection to the standby SCADA (OK
or an error code).
|
A_BCONNREASON_0 through A_BCONNREASON_200
|
The current state of the connection to the standby
node. This is either "Established" or text describing the current
state.
|
A_BLOCALADDR_0 through A_BLOCALADDR_200
|
This is for the backup network connection. For TCP/IP,
displays the local IP address used to reach the remote node.
|
A_BPATHSTATUS_0 through A_BPATHSTATUS_200
F_BPATHSTATUS_0 through F_BPATHSTATUS_200
|
Status of the connection to the backup network path.
|
A_BREMOTEADDR_0 through A_BREMOTEADDR_200
|
This is for the backup network connection. For TCP/IP,
displays the IP address of the remote node.
|
A_CONNDIRECTION_0 through A_CONNDIRECTION_200
|
Indicates whether the connection is incoming or outgoing.
–>
if outgoing.
<–
if incoming.
<–>
if both outgoing and incoming.
|
A_CURACTIVENODE_0 through A_CURACTIVENODE_200
F_CURACTIVENODE_0 through F_CURACTIVENODE_200
|
Indicates if the active node is the primary or secondary
SCADA.
A 0 in this field indicates that the primary SCADA
is the active node; a 1 indicates that the secondary SCADA is the active
node.
|
A_FAILDISABLE_0 through A_FAILDISABLE_200
F_FAILDISABLE_0 through F_FAILDISABLE_200
|
Automatic SCADA failover state.
A 0 in this field indicates that automatic SCADA failover
is enabled if it is configured; a 1 disables automatic SCADA failover.
Manual failover is still possible.
|
A_FAILOVER_0 through A_FAILOVER_200
F_FAILOVER_0 through F_FAILOVER_200
|
This field is set to 1 on automatic or manual SCADA
failover. You must reset it to 0 to receive notification of subsequent
failovers.
You can read to this field to trigger an event on
SCADA failover.
|
F_FAILOVERMANL_0 through F_FAILOVERMANL_200
|
Total number of manual failovers to this node since
iFIX startup.
|
F_FAILOVERTOTAL_0 through F_FAILOVERTOTAL_200
|
Total number of failovers (automatic and manual) to
this node name since iFIX startup.
|
F_LANANYFAILOVER
|
Use this field to see if any connection has had a
LAN failover. It is set to a non-zero number, if any.
|
A_LANFAILDSABL_0 through A_LANFAILDSABL_200
F_LANFAILDSABL_0 through F_LANFAILDSABL_200
|
Enabled
in this field indicates that LAN Redundancy is enabled if it is configured;
Disabled
indicates LAN Redundancy is disabled.
Use this field to disable LAN Redundancy on a per
connection basis.
|
A_LANFAILOVER_0 through A_LANFAILOVER_200
F_LANFAILOVER_0 through F_LANFAILOVER_200
|
This field is set to 1 on LAN failover. You must reset
it to 0.
|
F_LANFAILOVERTOTAL_0 through F_LANFAILOVERTOTAL_200
|
Total number of automatic failovers to this path since
iFIX startup. Session losses that are re-established over the same network
path are not included.
|
A_LOCALNAME
|
Displays the local physical node name.
|
A_LOGICALNAME_0 through A_LOGICALNAME_200
|
Logical SCADA Server name for this connection. (Same
as A_LOGICALSCADA and retained for backwards compatibility.)
|
A_LOGICALSCADA_0 through A_LOGICALSCADA_200
|
Logical SCADA Server name for this connection.
|
A_LOGICALSTATUS_0 through A_LOGICALSTATUS_200
F_LOGICALSTATUS_0 through F_LOGICALSTATUS_200
|
Status of the connection to the logical SCADA (OK
or an error code).
|
A_NETNAME_0 through A_NETNAME_200
|
Name used to connect to the remote node. For TCP/IP,
it is the remote node name.
|
A_PCONNREASON_0 through A_PCONNREASON_200
|
The current state of the connection to the primary
node. This is either "Established" or text describing the current
state.
|
A_PLOCALADDR_0 through PLOCALADDR_200
|
This is for the active network connection. Displays
the local TCP/IP address used to reach the remote node.
|
A_PPATHSTATUS_0 through A_PPATHSTATUS_200
F_PPATHSTATUS_0 through F_PPATHSTATUS_200
|
Status of the connection over the primary network
path.
|
A_PREMOTEADDR_0 through A_PREMOTEADDR_200
|
This is for the active network connection. For TCP/IP,
displays the IP address of the remote node.
|
A_PRIMARYPATH_0 through A_PRIMARYPATH_200
|
Primary network path.
When using LAN Redundancy, it shows the paths per
connection. For TCP/IP, it is the IP address.
|
A_PRIMARYSCADA_0 through A_PRIMARYSCADA_200
|
Primary SCADA Server name for this connection.
|
A_PRIMARYSTATUS_0 through A_PRIMARYSTATUS_200
F_PRIMARYSTATUS_0 through F_PRIMARYSTATUS_200
|
Status of the connection to the primary SCADA (OK
or an error code).
|
A_PROTOCOL
|
Displays the current protocol (TCP/IP) that iFIX is
using for networking.
|
A_SCADASTATUS
F_SCADASTATUS
|
The status of the SCADA node: ACTIVE (1) or STANDBY
(2).
|
A_SWITCHSCADAROLE
F_SWITCHSCADAROLE
|
A request for change in state: ACTIVE (1) or STANDBY
(2).
NOTE: The user who is currently logged on must have rights to the Enhanced Failover security area in order to perform a manual SCADA node role switch.
|
F_ALLOWREMOTEWRITES
|
This field is 1 if remote nodes are allowed to write
to the NSD
fields on this node, or 0 if writes are not allowed.
|
A_CURACTIVENODE_0 through A_CURACTIVENODE_200
F_CURACTIVENODE_0 through F_CURACTIVENODE_200
|
Indicates if the active node is the primary or secondary
SCADA.
A 0 in this field indicates that the primary SCADA
is the active node; a 1 indicates that the secondary SCADA is the active
node.
You can write to this field to perform a manual failover.
|
F_FAILDISABLE_0 through F_FAILDISABLE_200
A_FAILDISABLE_0 through A_FAILDISABLE_200
|
SCADA Server failover state.
A 0 in this field indicates that SCADA Server failover
is enabled if it is configured; a 1 disables SCADA Server failover. Manual
failover is still possible.
You can write to this field to disable automatic failover
to the standby SCADA on a per-connection basis.
|
A_FAILOVER_0 through A_FAILOVER_200
F_FAILOVER_0 through F_FAILOVER_200
|
This field is set to 1 on automatic or manual SCADA
failover. You must reset it to 0 to receive notification of subsequent
failovers.
You can read to this field to trigger an event on
SCADA failover.
|
F_FAILOVERMANL_0 through F_FAILOVERMANL_200
|
Total number of manual failovers to this node since
iFIX startup.
|
F_FAILOVERTOTAL_0 through F_FAILOVERTOTAL_200
|
Total number of failovers (automatic and manual) to
this node name since iFIX startup.
|
F_LANANYFAILOVER
|
Use this field to see if any connection has had a
LAN failover. It is set to non-zero if any F_LANFAILOVER_#
field is set to non-zero.
|
F_LANFAILDSABL_0 through F_LANFAILDSABL_200
|
A 0 in this field indicates that LAN Redundancy is
enabled if it is configured; A 1 indicates LAN Redundancy is disabled.
Use this field to disable LAN Redundancy on a per
connection basis.
|
A_LANFAILOVER_0 through A_LANFAILOVER_200
F_LANFAILOVER_0 through F_LANFAILOVER_200
|
This field is set to 1 on LAN failover. You must reset
it to 0.
|
F_LANFLOVRTOTAL_0 through F_LANFLOVRTOTAL_200
|
Total number of automatic failovers to this path since
iFIX startup. Session losses that are re-established over the same network
path are not included.
|
F_SCADAANYFAILOVER
|
Use this field to see if any connection has had a
SCADA failover. It is set to non-zero if any F_FAILOVER_#
field is set to non-zero.
|
F_SCADAREDUN
|
This field is set to 1 if Enhanced Failover is enabled;
it is set to 0 if it is disabled.
|
F_TRANSACTTIME_0 through F_TRANSACTTIME_200
|
Indicates the amount of time, in milliseconds, that
it took this iClient to get data from the SCADA Server the last time data
transfer occurred.
|