Updating the Spreadsheet Data

To automatically update spreadsheet data:

  1. In the Database Manager, in Ribbon view, on the Home or View tab, in the Settings group, click Options.

- Or -

In Classic view, on the View menu, click Options.

The Options Dialog Box appears.

  1. From the View Options area, select Enable Spreadsheet Auto Refresh.
  2. In the Enter refresh period field, type in the refresh rate you want.

IMPORTANT: Be aware that for a large database, you should increase the refresh rate to 20 or more seconds. Do not use the default of 5 seconds for large databases. If you leave the refresh rate at low number, such as the default of 5 seconds, and you try to import a large amount tags, the database may appear unresponsive.