Digital Alarm Block – Typical Uses

You can use the Digital Alarm block to:  

  • Detect alarm conditions of a digital state (either level or transition).
  • Represent items such as limit switches, valves, alarm contacts, or motor auxiliary contacts.
  • Assign descriptive labels to digital values through the Open (Labels) and Close (Labels) fields to make them more meaningful to the operator.
  • Define the alarm value and priority for the block.
  • Close a digital block when an alarm condition occurs.
  • Re-issue an alarm within the time defined in the Re-alarm Time field, as long as the block is still in a valid alarm state OR the Re-alarm Time is not disabled.
  • Suspend alarm processing within this block or multiple blocks based on a process condition.
  • Acknowledge alarms from a remote site.
  • Enable a block to attempt to write the contacts with every scan, even if the value being written is unchanged.
  • Separate the original alarm condition from the COMM alarm, and return the DA block to the same state as it was prior to a COMM alarm.
  • Assist in control situations such as direct digital control when chained to a PID or On-Off Control block.
  • Pass values to other blocks through the Next Block field.