Sets the bit of the specified register. This command is used only with
the SIM driver provided with iFIX. SIM registers range from 0 to 2000
and bits range from 0 to 15.
Syntax
SETF register:bit
Example
To set the 15th bit in the fifth SIM register to 1, enter: