Calculation Block – Equations

In order for the Calculation block to compute its output correctly, you must enter an equation. In general, the equation syntax is:  

input operator input

where input is one of the block's inputs and operator is a mathematical symbol. You specify inputs in the equation by their letter. For example, if you enter DI1 into the Calculation block's B Input field, you would refer to it in the equation as B.

You can enter any operator listed in the following table:

Operator

Function

ABS(input)

Absolute value

SQRT(input)

Square root

EXP(input)

Anti-log

LOG(input)

Natural log

LOG10(input)

Base-10 log

INT(input)

Changes floating point values to integers

-

Unary minus (example, -A).

^

Raise to power, exponential.

*

Multiply

/

Divide

+

Add

-

Subtract (example, A-B)

<

Less than

>

Greater than

NOTE: When doing greater than or less than comparisons, the Calculation block passes a value of 1 to the next block if the statement is true. If the statement is false, the block passes a value of 0.