Boolean Block

Purpose

The Boolean (BL) block calculates a single true/false output from multiple inputs.

Features

The Boolean block:

  • Is a primary block.
  • Can be used as a stand-alone block.
  • Takes up to eight input values and calculates a single output value.
  • Can use alarm states as inputs.
  • Can be used in a chain with time-based or exception-based processing.

See Also

Typical Uses

Example