For security reasons, you may want to restrict access to the recipes you create. Once you assign a security area to a recipe, it can only be opened with the Recipe Builder if the logged in user has rights to that security area. For example, if you assign security area A to the sample recipe, an operator who wants to open it must have rights to that security area.
To select a security area for a recipe, complete the Security Area group box. This group box defines the security area for the recipe. By default, the security area is set to NONE.
To select a security area for the
current recipe:
- On the Options menu, click Advanced Options. The Advanced Options dialog box appears.
- In the Security Area group box, enter the appropriate text as indicated below. You can enter up to 20 alphanumeric characters into the group box.
- To assign the recipe to every security area, type ALL.
- To assign the recipe to no security area, type NONE.
- To assign the recipe to a specific security area, type the security area name in the group box.
If you prefer, click the browse (...) button and select a security area from the dialog box that appears. Use the scroll bar or arrow keys to locate the security area you want. Press the OK button to complete the selection.