Syntax
variable = value
Recognized by
The Recipe Download program.
Description
An override parameter enables you to temporarily override a variable's formula. While the Recipe Download program does not limit you to the number of override parameters you can include, the command line can only be 128 characters. To use a command line longer than 128 characters, specify the override parameters in a text file and download these values with the Command Line File parameter.
Example: Override Parameters
To override the value of the variable #TEMP from 50 to 65 use the following text in the command line:
#TEMP=65