Opening a Recipe from the Operations Window

You can only open control recipes located in the control recipe path from the Recipe Operations window by selecting the Open command and displaying the Open Control Recipe dialog box.

This dialog box displays the following controls:

Recipe list box — displays the control recipes you can open.

Recipe Name field — allows you to enter the name of the control recipe you want to open.

Open button — opens the control recipes you selected from the Recipe list box or that you entered in the Recipe Name field.

To open a recipe from the Recipe Operations window:

  1. On the File menu, click Open. The Open Control Recipe dialog box appears.
  2. Select the recipe you want to open from the list box and select the Open button. The Recipe Builder opens the recipe and displays it on the screen.

    If you prefer, in the Recipe Name field, enter the name of the recipe and click Open, or double-click a recipe name. Regardless of the method you choose, the Recipe Builder opens the recipe and displays it on the screen.

How Do I...